Part Number: HD3SS3220
Other Parts Discussed in Thread: TUSB322I, TMUXHS4212, TUSB321AI
Hi,
There is stocks problem for the HD3SS3220, Is there alternative part for that?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: HD3SS3220
Other Parts Discussed in Thread: TUSB322I, TMUXHS4212, TUSB321AI
Hi,
There is stocks problem for the HD3SS3220, Is there alternative part for that?
Thanks.
I can see that TUSB3210LAI and TUSB322I are also on long lead time.
is there other combinations?
sizing matter, so solution that includes a FET for the SBUS it preferred. (only 5V needed, and only from my board to the device)
note that the solution still need DRP option.
Are you looking for CC controller only or are you open to PD controller solutions as well?
This is my first USB 3 and C design. searching for the difference between CC and PD jumped to your answer here:
I don't need PD, my design is for a nvidia Jetson that will have USB 3 Type C. the devices to connect the Jetson to are either Flash drive and mouse/keyboard. I don't need to increase the voltage, maybe only the current to 2/3A.
Edited: do I must have PD to change the Jetson rule? host/device?
No you do not need a PD controller for DRP function. If a CC controller with DRP function is what you need your options are limited to TUSB321AI and TUSB322I (both devices are used for USB 3 USB-C designs). Our CC controller solutions with integrated power path are source only.