Part Number: DS90UB940-Q1
Hi Team,
Could you kindly help to check 940 SHC review?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Amelie,
Sure. There are schematic and layout requests ahead of you. I will get back with you by 1/20.
Aaron
Hello Amelie,
here is my feedback to the 940N Schematic review:
- It looks like on all VDDxx pins, the 10uF capacitors are missing. Please refer to figure 38.
- Also make sure that on each VDDxx pin to have a capacitor between 10nF to 100nF directly on each pin.Please refer to figure 38.
- On CAP_I2S pins you just need 1 capacitor with a value between 10nF to 100nF. Please refer to figure 38.
- BISTEN and BISTC pins, If unused, tie to an external pulldown.
- Please make sure to maintain the correct power-up sequence and timing parameters, as per d/s section "9.1 Power-Up Requirements and PDB Pin".
- All GPIOs, If unused, tie to an external pulldown.
- CMLOUT pins, before terminating them, each pin shall be connected through an AC-Coupling capacitor. Please refer to d/s figure 38.
- For MODE_SEL0 & 1, please refer to table 7 and Table 8.
- Pins 49, 64 are reserved pins. May left as No Connect.