Part Number: DS90UB947-Q1
Other Parts Discussed in Thread: SN65DSI85, DS90UB948-Q1
Hi,
I have an existing design that uses the SN65DSI85 to create an LVDS output to two displays. I would like to transmit this LVDS over two serialized channels. Is the DS90UB947 compatible with the output of the SN65DSI85?
Today I have SN65DSI85 -> Display Driver
My idea would be: SN65DSI85 -> DS90UB947 -> 2 x Coax -> DS90UB948-Q1 -> Display Driver
Would that work in theory? My main question is if the input of the DS90UB947 is compatible with the SN65DSI85? Then is the output of the DS90UB948 going to be the same as the output from the SN65DS85 so my displays will work? Right now I don't have the choice of removing the SN65DSI85 from the system.
Thank you