Part Number: TPS65987D
Hello,
We're attempting to test a TPS65987DDH chip on a custom PCB and having a bit of trouble getting an established USB contract going. We're using a TPS65987EVM as the DFP port to test power delivery. The custom PCB has sink PDOs of the default 5V/0.9A and our target PDO of 20V/3A.
The issue we're running into seems to be showing similar behavior to when we were testing two separate EVMs. The source device had its LEDs blink periodically every second or so (5V PDO LED, SSMX FLIP & USB3 LEDs). The issue previously was that the source PDOs weren't setup properly, but we've tested a sink and source EVM without issue now.
Would there happen to be any issues with the attached project files?
TPS65987EVM (Source):
TPS65987DDH_EVM_DFP_Adv.pjt
Custom PCB with TPS65987DDH chip (Sink):
ct-config.pjt