Part Number: DS90UH941AS-Q1
Hi team,
I have a question about the register related to Port1 when I configure the device as Single DSI input, Dual FPD-Link output.
It is described that BCC is only available for primary (Port 0?) in this configuration, but in that case does registers related to Port 1 need to be care or
just ignore?
For example, CRC_ERROR_P1_7:0 (back channel CRC error counter) is available for Port 1 in this configuration?
regards,