Part Number: TRSF3243
HI staff
Let me ask you a question at the data rate of TRSF3243.
The FEATURES in the data sheet (SLLS862A) has the following description.
「Supports Operation From 250kbit/s to 1Mbit/s」
Similarly, page 5 Switching Characteristics also has a description of 250kbit/s to 1000kbit/s with the min specification.
Users will use TRSF3243 at a data rate of ~115.2kbps.
Question
・The data rate is lower than 250kbs (min) described in the data sheet, is it okay to use (~115.2kbps) it?
・Also, if there is a problem, is there a device that I can introduce?
best regards
cafain