This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DX90UB934-Q1EVM

Hi
I am using the TI DX90UB934-Q1EVM
I am trying to connect the aardvark device and totalphase application to communicate with the camera connected to the TI.
Is there a certain steps that need to be followed for this communication to work.
So far I cannot communicate with the camera through totalphase using aardvark.

  • Hello,

    Is the issue you are having that you cannot communicate with the image sensor over the back channel?  Are you able to verify that you can communicate with the serializer over the back channel and that you have LOCK?

    If so you need to make sure that you program the I2C address of the remote sensor to the slave ID register 0x5D and alias it in register 0x65 so the 934 will send it over the back channel.

    Regards,

    Nick