This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: Please check splitter mode configuration

Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: ALP

Hi Ti supporter,

1 . 941-> 2 Des 948 -> 2 1920*720 panel, as folllow

2 . panel spec.

5008.COG-VLBJT024-01 (BOE 文件编号 CS3-SPM- S065_AV123Z7M-N14-2WP0) 12.3 FHD ADS module Product Specification_Rev.1.pdf

3 . reg config

(ti941_addr, 0x01,0x08); //Disable DSI
(ti941_addr,0x1E,0x01); //Select FPD-Link III Port 0
(ti941_addr,0x03,0x9A); //Enable I2C_PASSTHROUGH, FPD-Link III Port 0
(ti941_addr,0x17,0x9E);

(ti941_addr,0x06,0x59);
(ti941_addr,0x07,0x30);
(ti941_addr,0x08,0x32);  

(ti941_addr,0x0E,0x03);
(ti941_addr,0x0F,0x03);
(ti941_addr,0x4F,0x8C); //Set DSI_CONTINUOUS_CLOCK, 4 lanes, DSI Port 0
(ti941_addr,0x5B,0x07); //Force Splitter mode
(ti941_addr,0x56,0x80); //Enable Left/Right 3D processing to allow superframe splitting

(ti941_addr,0x1E,0x02); //Select FPD-Link III Port 1
(ti941_addr,0x03,0x9A); //Enable I2C_PASSTHROUGH, FPD-Link III Port 1
(ti941_addr,0x17,0x9E);

(ti941_addr,0x06,0x61);
(ti941_addr,0x07,0x30);
(ti941_addr,0x08,0x34);  

(ti941_addr,0x0E,0x03);
(ti941_addr,0x0F,0x03);   
(ti941_addr,0x4F,0x8C); //Set DSI_CONTINUOUS_CLOCK, 4 lanes, DSI Port 1
(ti941_addr,0x5B,0x07); //Force Splitter mode
(ti941_addr,0x56,0x80); //Enable Left/Right 3D processing to allow superframe splitting

(ti941_addr,0x32,0x80); //Set the line size to 1280(LSB)
(ti941_addr,0x33,0x07); //Set the line size to 1280 (MSB)

(ti941_addr,0x1E,0x01); //Select FPD-Link III Port 1
(ti941_addr,0x36,0x00); //Set crop start X position to 0 (LSB)
(ti941_addr,0x37,0x80); //Set crop start X position to 0 (MSB) and enable cropping
(ti941_addr,0x38,0x7F); //Set crop stop X position to 1919 (LSB)
(ti941_addr,0x39,0x07); //Set crop stop X position to 1919 (MSB)
(ti941_addr,0x3A,0x00); //Set crop start Y position to 0 (LSB)
(ti941_addr,0x3B,0x00); //Set crop start Y position to 0 (MSB)
(ti941_addr,0x3C,0xCF); //Set crop stop Y position to 719 (LSB)
(ti941_addr,0x3D,0x02); //Set crop stop Y position to 719 (MSB)

(ti941_addr,0x1E,0x02); //Select FPD-Link III Port 1
(ti941_addr,0x36,0x00); //Set crop start X position to 0 (LSB)
(ti941_addr,0x37,0x80); //Set crop start X position to 0 (MSB) and enable cropping
(ti941_addr,0x38,0x7F); //Set crop stop X position to 1919 (LSB)
(ti941_addr,0x39,0x07); //Set crop stop X position to 1919 (MSB)
(ti941_addr,0x3A,0x00); //Set crop start Y position to 0 (LSB)
(ti941_addr,0x3B,0x00); //Set crop start Y position to 0 (MSB)
(ti941_addr,0x3C,0xcF); //Set crop stop Y position to 719 (LSB)
(ti941_addr,0x3D,0x02); //Set crop stop Y position to 719 (MSB)

(ti941_addr,0x40,0x04); //Select DSI Port 0 digital registers
(ti941_addr,0x41,0x05); //Select DPHY_SKIP_TIMING register
(ti941_addr,0x42,0x18); //Write TSKIP_CNT value for 300 MHz DSI clock frequency
(ti941_addr,0x01,0x00); //Enable DSI
(ti941_addr,0x30,0x01);
(ti941_addr,0x1E,0x07);

4. 941 dsi timing

Please help to check the splitter mode configuration ,thanks.

  • Hi Jianlin, 

    That is correct, we should be seeing DE and VSYNC signals as well, in single display mode. Especially if display is properly outputting!

    There is also a similar debug mechanism for 948 side, maybe we could try putting 948 in that mode and see if all 3 signals are populating. Lets be 100% sure though that correct pins were probed. Since display is outputting correctly, I'd expect these signals to be populating. 

    Sync Events Packet Structure.

    You mentioned in above reply that you were using sync event packet structure. Is this the case? 

    Regards, 

    Logan