Hi team,
In Dual Link mode, can I use D_GPIO as either input or output of DS90UH941AS-Q1?
Or the direction of D_GPIO is only DES to SER?
Could you advise how to configure below GPIO_1 amd GPIO_2_Config Register (0xE) [6:4] if I want to configure as below?
A : UH941 D_GPIO2 as input UH948 D_GPIO2 as output
B : UH941 D_GPIO2 as output UH948 D_GPIO2 as input
x00 : Functional input mode, I2S_DC input
x10 : Tri-state
001 : GPIO mode, output
011 : GPIO mode, input
101 : Remote-Hold
111 : Remote-Default
regards,