Part Number: DS92LV2411
Other Parts Discussed in Thread: DS92LV2412
Hi Team,
I want to consult the pin function of DS92LV2411.
There is a pin function table on page 3 of the data table for DS92LV2411.
There is an item of "type" on the table, which says w / pull-down.
I can't find the description here in the datasheet.
Please tell me what it means.
Please tell me the following Q1 ~ Q4
Q1 What does "w /" mean?
Q2 "pull-down" refers to the built-in pull-down terminal? right?
Q3 What is the pull-down resistance value with built-in pull-down? (there is no specification in the data sheet)
Q4 the description of 8.3.2.10 DES-Strap Input pins of DS92LV2412 in the same data table is as follows:
" open (NC) for Low, no pull-down is required (internal pull-down)"
Similarly, when setting the low of the strap input pins with w / pull-down, it says that there is no need for external pull-down resistance.
However, with regard to the terminal of DS92LV2411, the necessity of external pull-down resistance is not specially recorded.
If w / pull-down like config pin is written on the terminal of DS92LV2411, set low on the input terminal.
Does it need an external pull-down resistor?
Or is there no problem with open like strap input pins?
Thanks for your clarification.
Regards,