Part Number: TCA9548A
Hi team,
For the TCA9548
1. Is there any impact if the rise time of I2C is higher than the datasheet? (pull up voltage 3.3V, frequency 400kHz, I2C rise time 390ns)
2. Is there any impact if the pull up resistor of SDA and SCL is smaller than the datasheet? (pull up voltage 3.3V, frequency 400kHz, pull up resistor 600 ohm)
Thanks a lot.
Matthew Chen