Part Number: TCAN4551-Q1
ALL HI!
I use tcan4551-q1 to design can-fd.As shown in the figure below, I should take ISUP = 180mA as the current reference when designing the power supply? Or 90mA as a reference? If 180mA is taken as a reference, when I input 12V Vsub, the internal LDO will generate nearly 1W power consumption. Will the chip be too hot?I didn't see the description of LDO parameters in the manual. thank you!