Other Parts Discussed in Thread: TPS25833-Q1, TPS25831-Q1
Hi Kuno,
As you know TPS25832A-Q1 does not have Auto DCP Mode. Only it has CDP and SDP Modes with respect to BC1.2. I wish this chip had "Auto DCP Mode" feature.
Max. current limit is 500mA/900mA in SDP
Max. current limit is 1.5A in CDP.
According to SDP and CDP mode rules, cannot I set the current limit 3 Amper to Type-C port?
I a little bit confused.
My board is going to have only dedicated Charging Port feature, no data transfer. How can I set the ic to only DCP Mode?
Regards,
Mehmet COBAN