Part Number: DS90UH941AS-Q1
Other Parts Discussed in Thread: USB2ANY, ALP
Hi
my customer is using several ser/des on his board, when connecting the USBANY only one appear or is detected.
customer comment:
I’m trying to read the registers from the IC U8 (DS90UH941), address 0x1A, which are hanged in the same I2C bus with other 3 TI devices (1x DS90UH941[0x18], 1xDS90UH949[0x0C] and 1xDS90UH940[0x2C]).
The USB2ANY is only seeing the DS90UH949 with address 0x018!?.... see below.
Could you help me? How I can choose the I2C address if it has 2 different addresses for the same device type?
I’m using the I2C bus pulled to 1V8.
Only the DS90UH949 is pulled to 3V3.
regards,
Kamal