Part Number: TUSB8041A
Other Parts Discussed in Thread: TPS55288, INA230, TPS65987D, , TAS5805M, TUSB8041
Hello,
The I2C pins 37 & 38 have an internal pull-down resistor of min 14.5k. This requires a low-impedance pull-up resistor to achieve enough high-level.
On the other hand, the pull-up resistor impedance must be high enough in order to be pulled low. For this device low level is 0.4V @4mA and there are some other devices (in my system) that are even more limited in drive capability.
This limits the range of pull-up resistors just to get DC operation OK, for sure over a range of conditions and some series resistance due to switches, connectors and cabling in a system.
Is there any way to disable these pull-down resistors? We are configuring the device from an MCU so not with an EEPROM. This is because of BOM & testtime cost.
Kind regards,
Mark