Part Number: AM26LV31E
Hi,
I am designing a new design and have chosen to use with AM26LV31EIRGYR component for:
- 3 X RS422 outputs
- 1 X RS485 output
Is the component compatible for use with the RS485 standard too?
Regards,
Mor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The electrical characteristics are guaranteed only for a RS-422 load (at least 2 V over 100 Ω).
An RS-485 driver would be required to output at least 1.5 V over a 54 Ω load. It is likely that the AM26LV31E can do this, but there is no guarantee. However, differential receivers can work with at most 0.2 V, so in the worst case, you have just a reduced noise margin.
RS-422 and RS-485 have slightly different limits for bus voltages.
Hi Mor,
Clemens said it perfectly. AM26LV31E is designed for the RS422 standard. This differential line driver is guaranteed to output a differential voltage of +/- 2V across a 100 ohm load. RS485 drivers are designed to drive a differential output of +/- 1.5V across 54 ohm load. It is likely the case that AM26LV31E can drive this type of load, but no guarantee.
RS422 or RS485 standardized receivers have a input sensitivity of +/- 200mV to determine if signal is HIGH or LOW. Like Clemens stated, you will have reduced noise margin using a RS422 driver for RS485 application.
Clemens stated that RS422 and RS485 standards have different limits for bus voltages. This is due to common mode range.
Max Common-Mode Voltage RS422: -7V to +7V
Max Common-Mode Voltage RS485: -7V to +12V
RS485 devices also have wider data rate ranges up to 50 Mbps, can support more devices on the same bus, and receivers have higher input resistance.
Regards,
Tyler