Other Parts Discussed in Thread: TLK3131
Dear ,
is TLK3101 EOL ? whether to promote any part instead of TLK3101 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLK3131
Dear ,
is TLK3101 EOL ? whether to promote any part instead of TLK3101 ?
add a comments
because 3101 is 16bit wide parallel port, i need run 3.125Gbps, so 16bit wide can keep rate not high; TLK 3131 is 10 bit wide, FPGA need run 312.5M , then i could not control well, and TLK3131 integrates many application mode , it is complex , so need you help me give me a suitable promotion,many thanks~
Also, if there is LVDS transceiver can meet 3.125Gbps , it is also OK, but need consider cost