Part Number: DP83TC811S-Q1
Other Parts Discussed in Thread: DP83TC811EVM
Hello,
I designed the schematic according to the DP83TC811EVM to realize 100BASE-T1 to 100BASE-TX conversion, the hardware configuration are as attached files.
LD2021-PMMS-SYYN-V1.1 .pdf83TC811 configuration.xlsx
If the default circuit could realize the conversion, not through MDC/MIDO port? But the RX_CLK has 2.5MHz output,RX_CLK has no output.
In addition, if the autonomous mode means it may not configure the registers without MSP430?

Best regards
Kailyn