Other Parts Discussed in Thread: DS90UB935-Q1
Hi All,
I am trying to connect DS90UB935-Q1 and DS90UB964-Q1.
In this case, which of the following should be set for DS90UB964-Q1?
Best Regards,
Ishiwata
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
I am trying to connect DS90UB935-Q1 and DS90UB964-Q1.
In this case, which of the following should be set for DS90UB964-Q1?
Best Regards,
Ishiwata
Hello Ishiwata,
actually the UB964 is designated to be paired with a DVP SER, such as UB913A or UB933. Nevertheless, it can also be paired with a CSI SER such as the UB935, but you need to set this SER into the DVP mode as per this app note.