Hello Team,
My customer wants to configure USB-C-PD-DUO-EVM as Type-C PD sink.
If they use standard sink file available, then getting below notification-
He is using latest tool 6.1X but the sink board file created version is 4.01.
We tried using the option Project> Import setting of the project.
In the configuration tool, which is the correct option from below to configure the device as PD sink?
Or Can you share the sink board file generated using 6.1 version?
Regards,
Mahendra