This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUXHS4412: Interface with USB3.0

Part Number: TMUXHS4412

Hi

We are developing USB 3.2 tester . Our FPGA is not supporting Rx Detect on the Host side. We have planned to use mux circuit to detect the device attached in the Bus.

For Rx detection. We are sending 0.6V short pulse and measuring RC constant to check device is attached or not.

Is the TMUXHS4412 mux a pass through signal or it will affect in common mode voltage?

Can I get TINA Library module for TMUXHS4412?

Thanks,

Sankar.K