In two different setups, we are experiencing occasional bit inversions in the IP and MAC address of Ethernet packets sent through the EVM. The connection is:
PC(100base-tx full)->EVM->EVM->100base-tx switch->ethernet device. Here is a wireshark capture showing the type of problems we see:
I have followed instructions in the EVM manual, I can connect the USB2MDIO tool and set this register as indicated and read it back:
Do you know how to deal with the occasional bit inversions?