Part Number: SN65HVD1780
Other Parts Discussed in Thread: THVD2410, THVD2450
Hello Team,
My customer needs confirmation about the device SN65HVD1780 in a 3.3V supply. They wanted to confirm if can the transceiver still have up to 320 nodes with only a 3.3V power supply? In the datasheet, it says up to 320 node, but they assume this is for a 5V power supply. The datasheet says, "These devices are fully compliant with ANSI TIA/EIA 485-A with a 5-V supply and can operate with a 3.3V supply with reduced driver output voltage for low-power application"
Thanks in advance.
Regards
Renan