Part Number: TLK2711-SP
Hello,
I'am using the TLK2711-SP in a new design. Now, i have one question to the power up behavior.
In the powerup diagram of the TLK2711-SP (I am using the datasheet TLK2711A-SP, FEBRUARY 2018) it seems that:
ENABLE need to be "1"
GTX_CLK need to be running
LCKREFN need to be "1"
prior to power up the supplies.
Is this procedure necessary for the power-on reset ?
Thanks in advance
Mario