Part Number: DS90LV028A
Other Parts Discussed in Thread: TS3USB221
Hello team,
Is there a problem if LVDS signals are applied to the device without the device being powered?
Regards,
Carlo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90LV028A
Other Parts Discussed in Thread: TS3USB221
Hello team,
Is there a problem if LVDS signals are applied to the device without the device being powered?
Regards,
Carlo
Hello Malik,
If the device is powered down, how can its output be high?
Regards,
Carlo
Hi Malik,
Thank you for your support so far. Carlo directed me here to discuss a follow-up topic with you.
In our design, the LVDS signals are generated by an FPGA which is powered independently from the circuit containing the receiver. The receiving circuit is supposed to turn on shortly after the FPGA. Therefore, the 1.2 V common mode voltage is present on the LVDS lines before the receiver is up. In the current prototype this does not cause any isssues but we wanted to make sure that this is safe. As it appears not to be within the specification of the receiver, do you see any solution other than making sure that the FPGA is not powered until the DS90LV028 is powered?
Thank you, Jelle
Hi Jelle,
It is good to know that there is no functional issue here however it is hard to saw what effect this could cause over time or various parts. Another solution here could be a simple mux can be used to connect the LVDS lines when DS90LV028A is powered. TS3USB221 is an example. Powering up the FPGA can work as well but may not be feasible.