Part Number: TPS25832A-Q1
Hi Kuno!
I hope you are doing well.
I read the referance design that you shared with me before. I am attaching the document to this mail.
temperature of the ic's quaite high even under room temperature condition. is this occured because of the circuit area? (38 mm x 41 mm) but the total pcb area is 70 mm x 50 mm.
By the way Kuno, all of these efficiency results calculated when both two side of Type-C active or only one side?
I am considering the thermal performance of the ic. I will do 2x15W Type-C Project. My board will have 57.5mmx60mm sizes and I will use a four-layer board with the copper thickness for the four layers, starting from the top of, 2 oz / 2 oz / 2 oz / 2 oz. Total thickness will be 1.6mm.
Do you foresee any thermal problem?
Best,
Mehmet ÇOBAN