Part Number: DP83869HM
Can you please provide the max current consumption information in SGMII to RGMII mode.
VDDA2P5 - 2.5V
VDD1P1 - 1.1V
VDDIO - 2.5V
VDDA1P8 - NC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83869HM
Can you please provide the max current consumption information in SGMII to RGMII mode.
VDDA2P5 - 2.5V
VDD1P1 - 1.1V
VDDIO - 2.5V
VDDA1P8 - NC
Hi Mani,
These parameters are not characterized and only estimates can be given. Note these should not be taken as a guarantee and should only be used as a reference.
In S2R mode, max currents are as follows:
VDDA2P5 -> 12mA
VDD1P1 -> 117mA
VDDIO2P5 -> 60mA
Thanks,
David