Part Number: TFP401A
Hi Team,
Customer wants to confirm the configuration when only even pixel used for TFP401A.
1. Is it correct to only connect QE[0:7], QE[8:15], QE[16:23] pin and not connect QO[0:7], QO[8:15], QO[16:23] pin if customer wants to use only even pixel?
2. If 1. is correct, datasheet says "Not used, and held low, when in 1-pixel/clock mode." for QO[0:7], QO[8:15], QO[16:23]. Should customer connects these pins directly to GND or better connect to GND through resistor? If resistor is needed, could you tell me the suggestion value for each resistor?
Thanks.
Regards,
Jo