Part Number: TL16C752CI-Q1
Other Parts Discussed in Thread: TL16C754C, TL16C2752, TL16C752C, TL16C752D-Q1
Hello,
Is the errata sllz058a applicable to the TL16C752CI-Q1 device?
Indeed, the errata is not mentioned in itsTechnical documentation section wheras it is for the TL16C752C, TL16C754C and TL16C2752.
In addition, this errata is unclear to me regarding when a stop bit is considered to be "short". Only an example is provided with no detailed explanation of the issue. I understand that the issue may appear when the device receives data at a slightly higher baudrate than its configured value. But can you please indicate a tolerance on the baudrate value which may be supported? Or provide more details on the issue to be able to determine the correct workaround in my application?
Thanks,
Nicolas