Part Number: DP83822I
Hi,
I am testing a scenario in which DP83822i PHY is not connected to an Ethernet controller, i.e. Tx, Rx and other pins are not connected to an Ethernet controller via RMII.
I can read from and write into its register using MDIO, but when I connect it to my PC via a network cable, Partner Capability is not set in Auto-Negotiation Link Partner Ability Register (ANLPAR) register and none of LEDs change their status. even the ethtool on PC does not show any change in link status.
I wanted to ask, if DP83822i can send and receive advertisement and configure itself even if no Ethernet Controller is connected to it via RMII interface? In another word, can a standalone DP83822i PHY advertise and configure itself in auto negotiation mode?
Thanks in advance