This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042GV-Q1: External ESD protection

Part Number: TCAN1042GV-Q1


Hi,

Can I avoid using external ESD protection circuitry while using TCAN1042GV-Q1 CAN IC as it has got internal protection up to +/-16kV.

Regards,

Sunney

  • Hi Sunney,

    This device offers a high level of ESD and bus fault protection to help improve system reliability and robustness. However, the decision to include external protection will depend heavily on the requirements of the system as a whole. For example, systems that intend to operate in particularly hard electrical environments may require higher levels of ESD protection to ensure system survivability. For systems with lower ESD requirements, it is certainly possible to rely on the integrated protection offered by TCAN1042. 

    Let me know if there's something specific I can elaboration on and if you have any more questions.

    Regards,
    Eric Schott

  • Thank you Eric for response. I will let you know once I am clear with the requirement.