Can the TCAN1044V be used as a CAN extender, similar to the AMIS−42770?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeffrey,
In order to use a standard transceiver like TCAN1044 as a bus extender, you will need to include arbitration logic on the digital signal lines between the transceivers. We have a reference design that I will link below that includes this logic. The reference design includes isolation between the two CAN buses, but this is not necessary if the goal is only to extend the bus.
Let me know if you have any questions on this design or the arbitration circuit.
Regards,
Eric Schott