This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: Phone doesn't charge after Barrel_Jack_Event

Part Number: TPS25750

Hello, 

we are using the TPS25750D to charge a USB-C device which works well.

In some cases the USB-C device is attached before Vin is applied to the TPS25750 (-> "dead-battery").

We have enabled barrel_jack_event and tied it to a GPIO. Even when we tie it to Vin (5V), the charging doesn't work, but the VBUS is switching between 0V and 5V.

The charging is enabled when the Vin is applied exactly when VBUS is low, but this is not practical of course.

Do you know what could be the issue?

Thank you and best regards,

Ambroise