Part Number: DS100MB203
I'm trying to configure the MUX input/output selection via SMB
SEL0 and SEL1 are connected to pull-down, so default input/output selection is set by HW - port B for both
ENSMB is also connected to pull-down
To change the connection to PORT A, I perform the following:
Set ENSMB to '1' (3.3V GPIO)
set register 0x06 to 0x18
set register 0x5E to 0x06
set register 0x5F to 0xF0
It does not work
Moreover, when setting ENSMB all input are invalid
I changed SEL0, SEL1 connection in HW to pull-up and the input did changed to PORT A for both - excluding HW issue
Please advise
Thanks,
Anat