Part Number: TPS65987D
Other Parts Discussed in Thread: TUSB564
Hi Team,
I'm using the TPS65987EVM + 10G-EXPANSION-EVM (sink module). The DP output is working, but the USB3 over the Type-A connector doesn't work.
I checked it with an USB 3.0 mem-stick:
=> in the device-manager it is shown as "Unknown USB Device ( Problem at resetting the port)". It is also not detected as a USB2.0 device.
=> If I plug in an USB 2.0 mem-stick it is detected and shown in the device-manager and in Explorer.
Studying the forum I found the following thread: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/771713/tps65987d-tps65987-90evm-and-tps65987evm
I tried the settings of the "87D EVM Sink Board.pjt" provided in the answer => DP-output works, USB 3.0 output doesn't work
I also build a new project (please find attached), 87D_Sink-Only_DP-Alternate_NE01.pjt but the result is the same, DP-output works, but USB 3.0 doesn't work.
Please also find attached picture of the setup.
I'm looking forward to any hint.
Thank you very much for your efforts.
Regards
Norbert