Part Number: TPS23881
Other Parts Discussed in Thread: TPS23882B, TPS23882, TPS23880, , TPS23841, TPS2384, TPS23861
Hi,
Good morning. Our objective is to incorporate PoE to our device. Our use case is such that our device could connect to a single class 1 PD (4W max). We have run through selection guide but could not come to a firm decision on which component to use. So far our selections shows that most of the PSE controller allow connections to 4 and 8 PSE ports.
Would like advice on the follow questions -
1. Is there a PSE controller with a single PSE port?
2. How do we know if we should use 2 pairs or 4 pairs control? Since our target PD is a low power sensor of Class 1, it should not require 4 pairs. However, we could not confirm if the target PD is using either Pair 1-2. 3-6 OR Pair 4-5, 7-8. My reading shows that Endspan is based on Pair 1-2, 3-6 while Midspan Pair 4-5, 7-8. How do we design in such a way that we could cater for PD that uses Midspan or Endspan? Analog Devices seems to have a different definition of Midspan.
3. Would using a PSE controller for 4 pairs cater for PD that either uses Mid Span or Endspan?
4. What are the considerations of using TPS23882B in place of TPS23882?
5. What are the considerations of using TPS23881 in place of TPS23880?
6. The pricing for TPS23841 is very expensive at USD6.60. Is this an old chip?
7. TPS2384 is bigger and more expensive than TPS23882B. Is this a recommended chip as well?
8. TPS23861 is the cheapest among them all and with autonomous mode as well. Any concerns on using this chip?
Any information is much appreciated on this.
Best rgds,
Pang