Part Number: TPS65981
Other Parts Discussed in Thread: TUSB546A-DCI
We are having issue with this chip (configured as DFP role) where the HPD and AMSEL events are not being asserted when we connect a USB C Alt mode DP device. The internal register 0x58 indicates that the PD controller is entered in DP mode. Here is the register read from device ( 0x58), The first byte 0x03 is the byte 1.
0x03 0x01 0x00 0x00 0x00 0x08 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x05 0x10 0x00 0x00
This indicates DPModeActive = 1 and DP_SID_Detected =1. Which is DP device is detected. However as we already said, it does not assert HPD and AMSEL.
What else we need to do to make it work.