This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65981: HPD and AMSEL are not asserted

Part Number: TPS65981
Other Parts Discussed in Thread: TUSB546A-DCI

We are having issue with this chip (configured as DFP role) where the HPD and AMSEL events are not being asserted when we connect a USB C Alt mode DP device. The internal register 0x58 indicates that the PD controller is entered in DP mode. Here is the register read from device ( 0x58), The first byte 0x03 is the byte 1. 

0x03 0x01 0x00 0x00 0x00 0x08 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x05 0x10 0x00 0x00

This indicates DPModeActive = 1  and DP_SID_Detected =1. Which is DP device is detected. However as we already said, it does not assert HPD and AMSEL.

 

What else we need to do to make it work.