Part Number: DP83TD510E
Hello,
It's not clear to me from the datasheet whether Strap2 needs to be set high if you are in MII mode - or if it is a don't care. In MII mode you need RX_DV but is that guaranteed if you are in MII mode?
Mike.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TD510E
Hello,
It's not clear to me from the datasheet whether Strap2 needs to be set high if you are in MII mode - or if it is a don't care. In MII mode you need RX_DV but is that guaranteed if you are in MII mode?
Mike.
Hello Mike,
Strap2 is only used for RMII mode where you can program CRS_DV or RX_DV on pin18.
For MII mode, no strap will be needed on strap2 pin. RX_DV is guaranteed on pin 18.
Please let me know if you need more details.
--
Regards,
Gokul.