Part Number: TUSB4020BI
Hi,
I need to use TUSB4020BIPHP in my design, but unfortunately, I don't have 5V input. the upstream port comes from Intel Alder Lake CPU which sits on a motherboard, and it's delivered through a B2B controller to an Extension Board which I am designing. the B2B delivers only 3.3V.
internally I created the 1.1V through an LDO.
do I need to create the 5V from the 3.3V using a step-up converter?
BR,
Firas