This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925QSEVB: DS90UB925/DS90UB948 cannot transmit interrupt signal through INTB pin

Part Number: DS90UB925QSEVB

Hi team,

The customer's problem is described as follows:

The 925 / 948 works in the repeater mode, and the Host can already obtain the touch screen data, but the interrupt signal of the touch screen is connected to the BISTC / INTB_IN of the 948 and transmitted to the 925 through LVDS, and the 925 is connected to the host through the INTB pin. However, when the interrupt signal of the touch screen changes, the INTB pin cannot measure the signal change.

This interrupt connection method was also connected in other projects before, but it is not clear how to configure it. How do 925 and 948 need to be configured to transmit interrupt signals?

Best Regards,

Amy Luo