Part Number: DS90UB929-Q1
Hi team,
We have an application using DS90UB929-Q1 + DS90UB928-Q1.
However LCD just need about 15 MHz of pixel clock.
How does DS90UB929-Q1 work below 25 MHz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB929-Q1
Hi team,
We have an application using DS90UB929-Q1 + DS90UB928-Q1.
However LCD just need about 15 MHz of pixel clock.
How does DS90UB929-Q1 work below 25 MHz?
Hello,
The 929 has a minimum PCLK supported range of 25MHz so this will not work. In order to support this very low resolution LCD you would need to see if the panel can support a higher horizontal or vertical blanking to increase the PCLK >= 25MHz while maintaining the same active resolution
Best Regards,
Casey