Part Number: PCA9535
Other Parts Discussed in Thread: TCA9535, , TCA9555, PCA9555
Hello,
I am planning to use this device to drive an optocoupler (PN 140817143200). I am planning to drive it with a 12.5mA, so the total current of the octal will be within 100mA limit
For the Vcc I will use 5V. The questions are as follows:
1. Are there any issues Using Pn to drive optocoupler?
2. When I am going to set Pn pin Low, do I expect to see around 0.11V on the Pn pin according to the Figure 6-8 from datasheet at 12.5mA?
3. Is it a good practice to keep this 100k resistor across the optocoupler to reduce power consumption?
Here is an image of the driving principle

Best regards,
Timur