Part Number: DP83822I
Since customer's mechanical constrain, so they need to change the RJ45 connector's direction with 180degree on the PCB. With this change, the TX and RX wire could be exchanged for better layout routing.
As my understanding the auto-MDIX is able to support when crossover cable is being used, correct? if so, below pinout can be swapped when auto-MDIX is enable, correct? Very thanks.
TX+ => RX+
TX- => RX-
RX+ => TX+
RX- => TX-
Below is the connection plot.