Part Number: TLK2711-SP
Hello,
I would like you to confirm about below.
* According to datasheet section 8.2 functional block diagram, this device have two comma detect block for each 8bit data.
However, in fact, I believe that comma can be recognized by detecting both MSB and LSB data (Ex. MSB(15:8) K23.7, LSB(7:0) K28.5).
Is my understanding correct ?
What I want to confirm is user can not only use one of MSB or LSB channel.
Ex. User use only 8bit data (assigned to 7:0) and remained pin (15:8) is unused.
In that case, even if user input comma(K28.5) to LSB, since MSB is not used, device can not recognize comma.
Best Regards,