This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: SGMII Mode - Current consumption per rail in two supply mode

Part Number: DP83869HM

Hi,

I'd like to know the current consumption when using the SGMII mode per power rail on the configuration of two supply mode

VDDIO = 3.3V

VDD1P1 = 1.1V

VDDA1P8= NC

VDDA2P5 = 2.5V

  • Hi Eran,

    Please find the typical current consumption from each supply below.

    Supply Op_Mode Test Condition Typ Unit
    I(1V1) SGMII to Copper (1G) Room Temperature, 1.1V supply voltage 220 mA
    I(1V1) SGMII to Copper (100M) Room Temperature, 1.1V supply voltage 125 mA
    I(1V1) SGMII to Copper (10M) Room Temperature, 1.1V supply voltage 112 mA
    I(2V5) SGMII to Copper (1G) Room Temperature, 2.5V supply voltage 160 mA
    I(2V5) SGMII to Copper (100M) Room Temperature, 2.5V supply voltage 86 mA
    I(2V5) SGMII to Copper (10M) Room Temperature, 2.5V supply voltage 113 mA
    I(VDDIO=3.3V) SGMII to Copper (1G) Room Temperature, 3.3V supply voltage 16 mA
    I(VDDIO=3.3V) SGMII to Copper (100M) Room Temperature, 3.3V supply voltage 16 mA
    I(VDDIO=3.3V) SGMII to Copper (10M) Room Temperature, 3.3V supply voltage 16 mA

    Please let me know if you need more details.

    --
    Regards,
    Gokul. 

  • Hi Eran,

    Please let me know if you need more information. Else, please mark the query resolved.

    --
    Regards,
    Gokul.