This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS181: Input and output performance of TMDS181

Part Number: TMDS181


Hi team,

We are considering using the TMDS181 in ReTimer mode with a data rate of 1.48Gbps. I would like to know the following two points about above operation condition.

1.1.48Gbps input mask opening value
In Figure 13 (Input Eye Mask Post EQ - TTP2_EQ), the values in ps such as -33.7ps are for 6.0Gbps operation. What are the values of the voltage and time axes of the mask opening when operating at 1.48Gbps?

2.1.Maximum output jitter at 48Gbps operation
The maximum output jitter value when operating in ReTimer mode described in the datasheet is only for the condition of 3.4Gbps or higher. What is the maximum output jitter value for ReTimer mode in 1.48Gbps operation?

Best regards,

H.Tamiya