Hello team,
If you have the below information, can you share it with me?
*SN65LBC176-Q1 is being considered as an alternative for SN65LBC1801DRQ1.
1. ESD rating
2. Temperature characteristics for VIT+, VIT- and VOH, VO (-10℃~110℃)
3. Recommended typical circuit
4. Absolute minimum rating for Vcc
5. Pin termination when R and RE are not required.
6. Pin termination when D and DE are not required.
Best regards,
Shotaro