This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: About bin file by GUI

Guru 21045 points

Part Number: TPS25750
Other Parts Discussed in Thread: USB-PD-CHG-EVM-01,

bin file difference.xlsx

Hi Team,

 

Our customer can't output the bin file normally.

Me and they are setting up the GUI with the same steps and version(7.0.2.1), OS(Windows).

However, bin file has a diff.

Please refer to the attached file.

(By the way, bin file is output by Generate Full Flash Binary).

 

-Case1: I set to Sink/27W without BQ by GUI. Then EVM can negotiate USB PD so VBUS is rise 9V.

-Case2: They set to Sink/27W without BQ by GUI. Then EVM cant negotiate USB PD so VBUS repeats 5V and below.

* EVM is USB-PD-CHG-EVM-01

 

We have two questions.

 

----

[Q1]

Bin file has a diff(Yellow line in bin file).

Does the difference affect EVM?

If yes, could you please let us know the specific difference?

(For example, Vbus level, function(Sink or Source) etc.)

----

 

[Q2]

Could you please let us know the cause of the difference in bin file?

(For example, PC setting etc.)

----

 

Regards,

Hide