Part Number: DS90UB962-Q1
Hi team,
For 964 and 962:
1. Could each CSI-2 lane reach to max lane rate (1.6Gbps) when we using 4 lanes at the same time? That is to say, is that 962/964 max output bandwidth is 1.6G*4=6.4Gbps?
2. How to calculate the FPDLINK rate with 962 or 964? Are they both fixed 3Gbps? I think 964 is only supporting DVP mode so it could only support a fixed fpdlink rate about 2 or 3Gbps? What about 962?
3. Besides, I know when customer is using 964, we should let them pair with 933 or 913, could 962 and 964 both support the following pclk transmission and each configuration we just want to use one input port.
- 1920*1080@60fps YUV
- 1920*1080@30fps YUV
- 1280*3840@25fps YUV